Manage security posture check rules
Manage security posture check rules, including:
- Deleting a security posture check rule if it is no longer needed.
- Editing a security posture check rule if any setting needs to be updated.
- Duplicating a security posture check rule to quickly create similar rules.
Prerequisite
Make sure that you have the following permissions:
- View Security Posture Check Rule
- Configure Security Posture Check Rule
To configure permissions, go to
FactoryTalk Administration Console
> Policies
> Product
Policies
> FactoryTalk AssetCentre
> Feature Security
>
Security Compliance Policies
.To manage a security posture check rule
- OnSecurity Compliance, selectManage Security Posture Check rules.
- Do the following:
- Edit a security posture check rule:
- Select the rule that you want to edit, and then change the settings as you desire.
- SelectOK.
- Delete a security posture check rule:
- Select the rule that you want to delete, and then select
. - SelectYes.
- SelectOK.
- Duplicate a security posture check rule:
- Select the rule that you want to duplicate, and then select
.A new rule with the same settings will be created. - Select a desired controller from the dropdown list, enter a product string, and then configure desired settings in the copied rule.
- SelectOK.
Provide Feedback