Column headings on the Source & Display tab

The following table shows the column headings on the
Source & Display
tab and their meanings.
Column Headings
Description
Column Name
Shows each field of data in the selected data source. Drag to set their order in the search results report.
The rows shown under the column name vary depending on the data source that you are searching. For example, to sort the result by user name followed by logged time, place
User Name
as the first row and
Logged Time
as the second row.
Show
Shows the data source's selected data fields in the search results. In the
Show
column, select the checkbox for each field of data to show in the search results.
Sort
Selects the shown data fields to sort the search results. In the
Sort
column, select the cell to set the desired sort order, including ascending, descending, or no sorting. Columns are sorted in the order in which they are shown.
Width (%)
Specifies the column width of data fields in percentage in the search results. In the
Width (%)
column, select the cell to enter an integer as the percentage of width for a column.
The total of each column's width percentage can be equal to or less than 100 percent, but cannot exceed 100 percent. When the total of width percentage is less than 100 percent, all the columns except for the last one will keep their width percentage. The last column will expand its width by the percentage that is missing from 100 percent against the total of the rest column widths.
For example, there are a total of four columns, each of whose column width is 10 percent. In the search results, the first three columns take the space of 10 percent of the entire row, while the last column will take the space of 70 percent of the entire row, even though it's specified as 10 percent.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal