Pin file or binder versions
Use the pin operation to mark a file or binder version as the master file.
Prerequisites
- To pin file or binder versions, you must have thePinpermission.
To pin a file or binder version
- OnAssets, expand the assets tree, and then select a file or binder with the version to pin.
- Select theHistoryorLabelstab, and then select the version.
- Select thePin Versionbutton.
- Complete thePindialog.The maximum length of a comment is 2500 characters.
- SelectOK.Pinned versions are marked with a pushpin icon on theHistorytab. If you pin a labeled version, the pinned file or binder version is also marked on theLabelstab.
Provide Feedback