Undoing Check Outs of Elements

Undo check outs of projects, libraries, controllers, programs, functions, and function blocks from a repository. Undoing a check out undoes all changes to the elements definitions since these were checked out. The elements are no longer checked out, but instead of updating the repository with the edited version,
Undo Check Out
reverts to the local version to the latest version from the repository.
When performing recursive operations, elements locked or checked out by other users are not modified.
From the
Application View
, perform version control operations for all elements. From the
Communication View
and
Equipment View
, perform version control operations for projects and controllers.
IMPORTANT: The
Undo Check Out
operation may take longer than expected for larger applications.
To undo a checkout of an element or project
  1. From the required view, select the element or project for which to undo the check out from the repository.
  2. From the
    File
    menu, point to
    Version Control
    , and then click
    Undo Check Out
    .
  3. In the
    Undo Check Out
    dialog box, indicate whether to perform a recursive undo check out including all sub-elements, and then click
    OK
    .
    The elements are replaced in the repository and display with the checked in icon in the
    Application View
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal