Getting the Latest Versions of Elements
Get the latest version for elements like projects, libraries, controllers, programs, functions, and function blocks. When getting the latest version, recursively replace all sub-elements from the repository. When performing recursive operations, elements locked or checked out by other users are not modified.
IMPORTANT:
Before getting a previous version for a
controller with binding changes, check out all controllers affected by these changes.
From the
Application View
, perform version control operations for all elements. From the Communication View
and Equipment View
, perform version control operations for projects and controllers.
TIP:
The
Get Latest
operation may take longer than
expected for larger applications.To get the latest version of elements
- From the required view, select the element for which to get the latest version from the repository.
- From theFilemenu, point toVersion Control, and then clickGet Latest.
- In theGet Latestdialog box, indicate whether to perform a recursive get latest version including all sub-elements and whether to keep or replace locally modified elements, and then clickOK.
Provide Feedback