REPEAT Statement
The REPEAT statement is an iteration structure for a group of Structured Text (ST) statements. The "continue" condition is evaluated AFTER any iteration
REPEAT Statement | |
|---|---|
Name | REPEAT ... UNTIL ... END_REPEAT |
Syntax |
|
IMPORTANT:
Because the virtual machine is a synchronous
system, input variables are not refreshed during REPEAT iterations. The change of state of
an input variable cannot be used to describe the ending condition of a REPEAT
statement.
Example
(* ST program using REPEAT statement *) (* this program uses specific "C" functions to read characters *) (* on a serial port *) str := ''; (* empty string *) nbchar := 0; IF ComIsReady ( ) THEN REPEAT str := str + ComGetChar ( ); nbchar := nbchar + 1; UNTIL ( (nbchar >= 16) OR NOT (ComIsReady ( )) ) END_REPEAT; END_IF;
To insert a REPEAT statement
- From theToolbox, drag theREPEATelement into the language container.
Provide Feedback