EXIT Statement
The EXIT is commonly used within an IF statement, inside a FOR, WHILE or REPEAT block.
EXIT Statement | |
|---|---|
Name | EXIT |
Meaning | exit from a FOR, WHILE or REPEAT iteration statement |
Syntax | EXIT; |
Example
(* ST program using EXIT statement *) (* this program searches for a character in a string *) length := mlen (message); found := NO; FOR index := 1 TO length BY 1 DO code := ascii (message, index); IF (code = searched_char) THEN found := YES; EXIT; END_IF; END_FOR;
To insert an EXIT
- In the language container, typeEXIT.
Provide Feedback