Assignments
The expression can be a call to a function.
Assignments | |
|---|---|
Name | := |
Meaning | Assigns a variable to an expression |
Syntax | <variable> := <any_expression> ; |
Operands | Variable must be an internal or output variable and the expression must have the same type |
Example
(* ST program with assignments *) (* variable <<= variable *) bo23 := bo10; (* Variable <<= expression *) bo56 := bx34 OR alrm100 & (level >= over_value); result := (100 * input_value) / scale; (* assignment with function call *) limited_value := min (16, max (0, input_value) );
To insert an assignment
- In the language container, type :=.
Provide Feedback