Building an AADvance Project
Choose to generate code and the necessary files for a project. Also, choose to build only a selected element within a project such as a controller or library.
When building projects, controllers, or libraries, view the progress of the build operation in the
Output
window. When the build operation is complete, view generated errors in the Error List
.
TIP:
- Always perform a build operation after getting a specific version of a project.
- Verify all elements are connected before performing a build.
Task | Procedure |
|---|---|
Build a project | In the Application View , right-click the project element, and then click Build All (or press Ctrl+Shift+B ). |
Build a selected element within a project |
|
View the build progress and generated errors |
|
Stop a build | Perform either of the following steps:
|
The
AADvance-Trusted SIS Workstation software
rebuilds controllers and increases the build number in these conditions:- The controller has been modified since the last compilation
- A dependent library is not compiled, was compiled after the controller, or was modified since the last compilation
- Contains a program organization unit (POU) needing compilation: a POU has been modified since the last compilation, a POU is an LD or FBD function block for which symbol monitoring is activated, and a POU has local array variables when array index verification is activated.
- The controller contains variables in binding consumer links or variables in CIP consumer links
The compiler generates different code for simulation than for targets. Specify the code for simulation in the controller properties before building.
Generating monitoring symbols information to graphically monitor the values of variables requires a significant amount of memory space. When compiling, an error message stating that the memory limit has been reached may display in the output window. To enable compiling, either disable monitoring for the POU, remove elements from the POU, or reduce the size of the POU.
Provide Feedback