Verifying POU Syntax
Verify the syntax for programs, functions, and function blocks. Verifying the syntax only verifies the programming syntax without producing code. View verification progress in the
Output
window.Task | Procedure |
|---|---|
Verify POU syntax | Before performing a build, ensure all elements are connected.
TIP:
After getting a specific version of a
project, clean and then build the project.
In the Application View , right-click the program, function, or function block, and then click Verify <POU> . |
View verification progress and generated errors |
|
Provide Feedback