TP
Increase an internal timer up to a given value.
Arguments | ||
|---|---|---|
IN | BOOL | If rising edge, starts increasing internal timer (if not already increasing) If FALSE and only if timer is elapsed, resets the internal timer Any change on IN during counting has no effect. |
PT | TIME | Maximum programmed time |
Q | BOOL | If TRUE: timer is counting |
ET | TIME | Current elapsed time. Possible values range from 0ms to 1193h2m47s294ms. |
Timing diagram

Provide Feedback