HYSTER
Hysteresis on a real value for a high limit.
Arguments | ||
|---|---|---|
XIN1 | REAL | Any real value |
XIN2 | REAL | To test if XIN1 has overpassed XIN2+EPS |
EPS | REAL | Hysteresis value (must be greater than zero) |
Q | BOOL | TRUE if XIN1 has overpassed XIN2+EPS and is not yet below XIN2-EPS |
Example of a timing diagram

Provide Feedback