Import an AADvance Project with Library with outdated Series 9000 Target Definition

If existing projects and their libraries were created using version 1.1 or 1.2 of
AADvance Workbench
use the following procedure to import the projects and their libraries.
To import an AADvance project with its library with outdated Series 9000 target definition
  1. Before importing the original project into
    AADvance® Workbench
    version 2.1, rename the library folder that contains the MDB file used by this project.
  2. Import the project. For more information refer to Import an AADvance Project.
    The
    AADvance® Workbench
    dialog box appears.
  3. If you are warned there is a Project Missing Files, select
    Yes.
  4. Select the project in the Application View and select
    File > Version Control > Check In
    .
    The Check-in Confirmation dialog box appears.
  5. Select
    OK
    .
  6. Import the project library, by using the Add New Library functionality. For more information refer to AADvance Libraries.
    The Security Password dialog box may appear. If it does, enter the password of the library again and select
    OK
    .
  7. Select
    FILE> Save All
    .
  8. Select
    FILE> Close Project
    .
  9. Import the now closed project. For more information refer to Import an AADvance Project.
  10. Right-click
    the newly imported project in the Application View and select
    Version Control > Check Out
    .
    The Check Out dialog box appears.
  11. Enable
    Recursive
    .
  12. Select
    OK
    .
  13. Select the project in the Application View and select
    File > Version Control > Check In
    .
    The Check-in Confirmation dialog box appears.
  14. Select
    Yes
    .
  15. Close and reopen the project.
  16. Right-click
    the new project in the Application View and select
    Version Control > Check Out
    .
    The Check Out dialog box appears.
    Enable
    Recursive
    .
  17. Select
    OK
    .
  18. Select
    Check in all checked items
    in the Pending Checkins panel.
    The Check-in Confirmation dialog box appears.
  19. Select
    Yes
    .
  20. Select
    PROJECT > Version Control > Archive
    .
    The Archive <project> dialog box appears.
  21. Select
    Latest Version
    from the Archive Mode dropdown.
  22. Select
    Archive
    .
    The Save As dialog box appears.
  23. Save the latest version of the project.
  24. Note:
    AADvance® Workbench
    version 2.1 is no longer required for the following steps.
  25. In
    AADvance-Trusted SIS Workstation software®
    , select
    FILE> New Project
    .
    The New Project dialog box appears.
  26. Select
    Restore
    from
    Project Types.
  27. Browse the Archive Path to the
    newly created VSC file
    .
  28. Select
    OK
    .
    The project is restored.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal