Defining a
Modbus
Slave

The AADvance controller can operate as a
Modbus®
slave, supporting up to a maximum of 10
Modbus
slaves on each processor module. A controller with three processor modules supports up to 30
Modbus
slaves.
TIP: As a
Modbus
slave device, the controller only transmits data upon a request from a
Modbus
master and does not communicate with other slaves.
When configuring a controller as a
Modbus
slave, select whether the slave uses a serial or Ethernet connection. The connection type affects the slave properties like the available protocols and ports.
To define a
Modbus
slave
  1. In the
    Communication View
    , expand the required controller, and then expand the
    Modbus
    element.
    The
    MODBUS Slave
    and
    MODBUS Master
    elements are displayed.
  2. Right-click the
    MODBUS Slave
    element, and then click
    Add New Slave
    .
  3. In the
    Communication View
    , double-click the slave instance, then in the
    Communication
    property page, select the connection type and define the required properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal