Update Ethernet ports of CIP produce and CIP consume links
After building the project, if the
Output
window displays a message indicating Multiple CIP network instances found
, update the Ethernet ports of CIP produce and CIP consume links.To update Ethernet ports of CIP produce and CIP consume links
- Clear all Ethernet ports of each CIP produce and CIP consume link.
- InCommunication View, double-click the CIP produce or CIP consume link.TheCommunicationproperty page displays.
- Clear all Ethernet ports in theCommunicationproperty page.TIP: Perform Step 1 on all CIP produce and CIP consume links.
- Save and then close the project.
- Open the project.
- Select the required Ethernet ports for each CIP produce and CIP consume link.
- InCommunication View, double-click the CIP consume or CIP produce link.TheCommunicationproperty page displays.
- Select the required Ethernet ports in theCommunicationproperty page.TIP: Perform Step 4 on all CIP produce and CIP consume links.
- Build the project.
Provide Feedback