Creating the
CIP
Produce Link

For a controller, create one
CIP
produce link for sending data to a remote controller across a
CIP
network. When defining a produce link, specify the Ethernet port connecting to the
CIP
network with the remote controller. Then map producer variables.
IMPORTANT: If the IP address of the producer is modified, update the path to the producer in the consume link.
To create the
CIP
produce link
  1. In the
    Communication View
    , expand the required controller, right-click
    CIP
    , and then click Add
    CIP Produce Link
    .
    The
    With Any
    link and
    CIP Produce
    item are added to the
    Communication View
    tree structure.
  2. Double-click the
    With Any
    link, then in the
    Communication
    property page, select the Ethernet port to use for communication with the
    CIP
    network.
    TIP: Your specified Ethernet ports also apply to all
    CIP
    Consume Links of this controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal