Using a Controller as an SNTP Client and Server
In a system with many AADvance controllers, configuring one controller as a client and server is helpful. The controller becomes the client of a hardware or software network time server and transmits the date and time to the other controllers configured as clients. A controller being both a client and server can reduce the load on the server when the clients are using unicast.
Provide Feedback