Configure a Controller as an SNTP Client
As an SNTP client, the AADvance controller accepts the current time from an external Network Time Protocol (NTP) or SNTP network time server.
TIP:
Always select both Ethernet ports of a processor slice
whether configuring SNTP as a client, server, or both. Also when only requires a primary
server.
The SNTP client receives the real time clock data from the primary network time server.
IMPORTANT:
Modifications to the SNTP settings are active
after the power has cycled.

The SNTP client settings provide this information to the controller:
Setting | Description |
|---|---|
Enable SNTP Client | The controller is configured as an SNTP client |
SNTP Client Mode | Operating mode for the time synchronization signal used by the processors for setting their real time clock:
|
Ethernet Port | Ethernet port of the controller |
SNTP Server IP Address | IP address of the network time server. Non-fault tolerant operations require one SNTP server for a processor. Other processors will automatically synchronize to the server and inherit the time. Fault-tolerant SNTP client operations require more than one server address. If only a primary time server is required, set the secondary time server IP address to the null value of 0.0.0.0. |
Required SNTP Version | The version of the SNTP server. Possible versions are SNTPv1 , SNTPv2 , SNTPv3 , SNTPv4 , or Any . When the version of the NTP/SNTP that the server offers is unknown, choose Any. This latest option disables some validation aspects of the incoming signal. |
To configure a controller as an SNTP client
- In theCommunication View, expand the required controller, and then double-clickSNTP.TheCommunicationproperty page displays.
- From theCommunicationproperty page, in the SNTP Client section, selectEnable SNTP Client.
- Specify theSNTP Client Modefor each server:
- To use the broadcast mode where the SNTP client passively waits for regular broadcasts from the server, from the drop-down combo box, clickBroadcast.
- To use the unicast mode where the SNTP client actively polls the configured servers and uses their responses, from the drop-down combo box, clickUnicast.
- Select the requiredEthernet Portsand then define theSNTP Server IP Addressproperty for the required servers.
- For a non-fault tolerant operation, define one SNTP server for only one processor. The other processors will automatically synchronize to the first processor and inherit the time.
- For a fault-tolerant SNTP client operation, define more than one server address.TIP: The first address represents the primary server and the second address represents the secondary server for each processor module. At start up, the SNTP client chooses the primary server of the lowest slice; if no primary signal is valid, the SNTP client looks for an active secondary server signal.
- Define theRequired SNTP Versionproperty for each required pair of servers for the processor modules.TIP: When the NTP/SNTP server version is unknown, use theAnyoption, disabling some validation aspects of the incoming signal.
Provide Feedback