Configure a Controller as an SNTP Server
The AADvance controller can fulfill the role of a primary or secondary SNTP server to provide a network time signal throughout the network.
TIP:
Always select both Ethernet ports of a processor slice
whether configuring SNTP as a client, server, or both. Also when only requires a primary
server.
SNTP servers operate in broadcast and unicast time synchronization signal modes. Specify a
directed broadcast address for an interface enables serving time on the interface for both
modes. This method of configuring is derived from the NTP configuration command language.
The directed broadcast address for an interface:
= ( (IP address for interface) bitwise-and (subnet-mask) ) bitwise-or (bitwise-not subnet-mask)
Example: if the IP address for an interface is 10.10.1.240 and its subnet-mask is 255.255.255.0, then the directed broadcast address is:
= ((10.10.1.240) bitwise-and (255.255.255.0)) bitwise-or (bitwise-not 255.255.255.0)
= (10.10.1.0) bitwise-or (0.0.0.255)
= (10.10.1.255)
IMPORTANT:
Modifications to the SNTP settings are active
after the power has cycled.

The SNTP server settings provide this information to the controller:
Setting | Description |
|---|---|
Enable SNTP Server | The controller is configured as an SNTP server |
SNTP Server Mode | Operating mode for the time synchronization signal used by the processors for setting their real-time clock. Configure the 9110 processor module as one of these:
|
Ethernet Port | Ethernet port of the controller |
SNTP Broadcast Address Mask | IP address for the interface. Setting the Broadcast IP Address to zero (0.0.0.0) for a processor disables the server on that interface. |
Broadcast Poll (seconds) | The broadcast polling time, in seconds. Possible values range from 4 to 1024; The default value is 10. |
To configure a controller as an SNTP server
- In theCommunication View, expand the required controller, and then double-clickSNTP.TheSNTPproperty page displays.
- From theSNTPproperty page, in theSNTP Serversection, selectEnable SNTP Server.
- Select the requiredEthernet Ports, and then define theSNTP Server Broadcast Address MaskandBroadcast Poll (seconds)properties for the required servers.
- To disable the server, set the IP address to 0.0.0.0
- For a non-fault tolerant operation, define one SNTP server for only one processor. The other processors will automatically synchronize to the first processor and inherit the time.
- For a system requiring a fault-tolerant operation, define more than one server IP address.
- Specify theSNTP Server Modefor each server:
- To use the unicast mode where the controller waits to be polled by a client and responds with a time signal without broadcasting any time signals, from the drop-down combo box, clickUnicast.
- To use the broadcast mode where the controller regularly broadcasts and responds to unicast polling requests on the network, from the drop-down combo box, clickBroadcast.
Provide Feedback