Configure a Slave for a
Modbus
Master

When configuring a slave for a
Modbus®
master, define these settings:
  • Configuration settings, communications and status reporting
  • Messages, messages list displaying all of the messages defined for a slave
  • Statistics data, time to complete a slave polling
mdb_mrslcfg
To configure a slave for a
Modbus
master
  1. In the tree structure, select the
    Modbus
    master, and then click
    Add Slave
    .
  2. (optional) Click
    Change Name
    and enter a name for the slave.
  3. Configure the properties for the slave:
    1. To configure the configuration settings, click the
      Configuration
      tab, and then define the properties.
    2. To configure the messages, click the
      Messages
      tab, and then define the properties.
    3. To configure the statistical data, click the
      Statistics
      tab, and then define the properties.
  4. Click
    Validate
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal