Report Statistics Data
To report statistics for a master, define these properties:
Property | Description | |||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Statistics Reporting | Modbus addresses for the data transmission variable and
control variable. For the data transmission variable, the value returned is an
integer which represents the poll time in 1/100th of a second. For the control
variable, the data type is either Boolean (coil) or integer (holding
register).Use different Modbus addresses for all control and status
holding registers, and control variable coils.
| |||||||||||||
Statistics Type | The type of statistics to record for the Modbus master:
|
Depending on the statistics type, the control variable performs a different function. For
Max Scan Rate
and Average
, a falling and rising edge sequence resets the
measurement.Statistics Type | Control Variable Value | Result |
|---|---|---|
Max Scan Rate | False -> True (Boolean) 0 -> non-zero (Integer) | Max value remains until next cycle completed. Max value then updated with time of next Max Scan Rate complete cycle. |
True -> False (Boolean) non-zero -> 0 (Integer) | Triggers a reset | |
Scan Rate | False -> True (Boolean) 0 -> non-zero (Integer) | No effect (data updated every cycle) |
True -> False (Boolean) non-zero -> 0 (Integer) | No effect (data updated every cycle) | |
Average | False -> True (Boolean) 0 -> non-zero (Integer) | Average value remains until next cycle completed. Average value then updated with time of Average next complete cycle. |
True -> False (Boolean) non-zero -> 0 (Integer) | Triggers a reset |
The master poll scan is defined as the time taken to poll all of the slaves defined for the
master. The first slave defined in the poll list is taken as the start and end point of the
timing sequence.
Sequence Number | Message | ||
|---|---|---|---|
1 | Slave 1 Msg 1 | ![]() | Master Poll 1 |
2 | Slave 2 Msg 1 | ||
3 | Slave 3 Msg 1 | ||
4 | Slave 1 Msg 2 | ![]() | Master Poll 2 |
5 | Slave 2 Msg 2 | ||
6 | Slave 3 Msg 2 | ||
7 | Slave 1 Msg 3 | ![]() | Master Poll 3 |
8 | Slave 2 Msg 1 | ||
9 | Slave 3 Msg 3 | ||
10 | Slave 1 Msg 4 | ![]() | Master Poll 4 |
11 | Slave 2 Msg 2 | ||
12 | Slave 3 Msg 1 | ||
13 | Slave 1 Msg 1 | ![]() | Master Poll 5 |
14 | Slave 2 Msg 1 | ||
15 | Slave 3 Msg 2 |
To report statistics data for a
Modbus
master- Click theStatisticstab, and then select theReport Statisticscheck box.
- In theStatistics Reportingarea, define theModbusaddresses for these variables:
- Data, application variable sending the data to the application
- Control, application variable performing a different function depending on the statistics type
- In theStatistics Typearea, select a statistics type:
- Max Scan Rate, the maximum scan time
- Scan Rate, the latest scan time
- Average, the average scan time
- ClickSave.
Provide Feedback