Serial Communications

Configure serial communications using the
Serial
tab in the
Com Port Options
dialog box. The available serial ports display in the
C
ommunication Ports
drop-down combo box. Leave the remaining settings at their defaults, unless the
Trusted®
System communications configuration has been changed. Selecting a serial port defines that port as the communication channel, regardless of the settings on the
Ethernet
tab.
sct_scps
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal