Ethernet Communications

Configure Ethernet communications using the
Ethernet
tab in the
Com Port Options
dialog box. If the
Trusted®
System has previously been configured for Ethernet communications (using the SYSTEM.INI configuration) then further communications are made quicker by Ethernet. On the
Ethernet
tab, enter the TCP/IP address assigned to the socket used on the communications module. Leave the port defined as 6000 unless changed in the SYSTEM.INI configuration.
sct_scpe
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal