Specify Cross Reference Browser settings
For
Trusted®
projects, customize the colors that display in the Cross Reference Browser including the colors for the grid rows, alternating grid rows, selected references, selected symbols, and more. The Cross Reference Browser automatically alternates colored rows with white rows.To customize the colors displayed in the Cross Reference Browser
- From the Tools menu, clickOptions.
- From the Options dialog box, expandCross Reference Browser Settings, then clickGrid Settings.
- Customize the required options, then clickOK.
- To change the colors applied to grid rows, alternate rows, selected reference rows, selected symbol rows, or other items, click the respective option, then select a color from the drop-down combo-box.
Provide Feedback