Specify Block Library settings

Specify the display mode for the
Block
Library
on startup. Display the
Block
Library
using expanders or tabs.
To adjust the display mode for the block library
  1. From the
    Tools
    menu, click
    Options
    .
  2. In the
    Options
    dialog box, expand
    Block
    Library
    Settings
    , then click
    General
    .
  3. In the
    Options
    dialog box, select the required display mode from the drop-down menu, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal