Specify Trusted settings
Trusted
settingsFor
Trusted
variables, specify the display format for the Modbus
address. The Modbus
address displays in hexadecimal or decimal format.To adjust the
Modbus
address format for variables- From theToolsmenu, clickOptions.
- In theOptionsdialog box, expandCAM, and then clickTrustedSettingsGeneral.
- Select the required display type from the drop-down menu, and then clickOK.
Provide Feedback