Edit Box Settings

Use the edit box settings to specify default values for the individual object properties.
To specify the default settings for edit box objects
  1. From the
    Tools
    menu, click
    Options
    .
  2. From the
    Options
    dialog box, expand
    ISaVIEW
    Settings
    , then expand
    ISaVIEW
    Object
    Settings
    , and then click
    Edit
    Box
    Settings
    .
  3. Specify the default values for the required properties, then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal