Gauge Settings
Use the gauge settings to specify default values for the individual object properties.
To specify the default settings for gauge objects
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandISaVIEWSettings, then expandISaVIEWObjectSettings, and then clickGaugeSettings.
- Specify the default values for the required properties, then clickOK.
Provide Feedback