Image Settings

Use the image settings to specify default values for the individual object properties.
To specify the default settings for image objects
  1. From the
    Tools
    menu, click
    Options
    .
  2. From the
    Options
    dialog box, expand
    ISaVIEW
    Settings
    , then expand
    ISaVIEW
    Object
    Settings
    , and then click
    Image
    Settings
    .
  3. Specify the default values for the required properties, then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal