Reset Visual Settings in LD POUs
Reset the visual settings to modify the visual properties for the language containers and elements in Ladder Diagram (LD) Program Organization Units (POUs).
After resetting the
LD Container
in the Properties
window, subsequent elements added to the language editor use the new values.To reset visual settings in LD POUs
- In an open LD POU, right-click in the rung, and then select one of these commands:
- Reset All Visual Settings- Resets the visual properties of all elements in the open POU to the properties defined for theLD Containerin thePropertieswindow.
- Reset Container Visual Settings- Resets the values defined for theLD Containerin thePropertieswindow to the values set inTools>Options>IEC Languages>Ladder Diagram (LD). Elements in the open POU are not modified.
TIP:
When changing the values in
Tools
> Options
> IEC Languages
> Ladder Diagram (LD)
, close and then reopen the software before using Reset All Visual Settings
or Reset Container Visual Settings
to apply the new values to the LD Container
properties.To reset visual settings for selected elements in LD POUs
- In an open LD POU, select the elements to reset, right-click and then selectReset Element Visual Settings.
The visual properties of the selected elements reset to the values defined for the
LD Container
in the Properties
window.Provide Feedback