Add redundancy-capable devices
Add specific or all redundancy-capable devices to the security policy
model.
Prerequisites
- Make sure that redundancy systems are correctly connected and configured. See Redundancy system.
- To add redundancy-capable devices
- To manually add a redundancy-capable device to the security policy model:
- Add a redundancy-capable device. See Add a device.
- InPROPERTIES, in port properties, selectValidate redundancy.
- To add a redundancy-capable device fromDiscoveryto the security policy model, see Add discovered devices.
- To configure redundancy-capable devices in the security policy model:TIP:Rockwell Automationrecommends configuring redundancy-capable devices in the security policy model if you make many redundancy changes to the security policy model at once.
- Validate the security policy model for redundancy. See Validate a policy model.
- InUpdate security policy model to ensure redundancy, review the suggested changes to the model and then update the model. See Dialog: Update security policy model to ensure redundancy.
For examples on how updates for redundant systems may impact a security policy model, see Examples: Security policy model updates for Redundant Chassis Pairs.
Inspect the redundancy status and perform any additional steps if
applicable. See Redundancy statuses.
Provide Feedback