Redundancy statuses
Configured redundant controllers may display these redundancy statuses.
Unknown
Case | User action |
---|---|
Device may be a part of a Redundant Chassis Pair | Validate redundancy. |
Device is a part of a Redundant Chassis Pair, but the primary or secondary IP
address exists in the security policy model | Validate redundancy in the security policy model to identify duplicated IP
addresses and follow instructions. |
Configured
Case | User action |
---|---|
Device is configured as a part of a Redundant Chassis Pair | N/A. The redundancy status is already verified. |
Not configured
Case | User action |
---|---|
Device not configured for redundancy | If needed, configure the device as a part of a Redundant Chassis Pair and then
validate the redundancy status for the device or the security policy model
again. |
Unable to create a Redundant Chassis Pair due to the current state of devices in
the security policy model. Either primary or secondary IP address of the Redundant Chassis Pair:
| Change the device IP address in the model or modify the IP address configuration
of the Redundant Chassis Pair and then validate the redundancy status for the
device or the security policy model again. |
Provide Feedback