Validate a policy model
Validate a policy model to confirm that all devices are operational and have network access.
- From the toolbar, selectValidateand then select either:
- CIP Securityto validate connections betweenCIP Securitysystem components.For more information, see CIP security policy.
- OPC UAto validate connections betweenOPC UAsystem components.For more information, see OPC UA security policy.
- (administrators only)CIP Redundancyto validate connections between Redundant Chassis Pairs.For more information, see Redundancy system.
TIP: You can stop the validation process at any time by pressingSTOP VALIDATIONin the status bar.Resultsdisplay any potential information messages, warnings, or errors. - (optional) Save the validation results by selecting.Save
Provide Feedback