CIP security policy

CIP Security
helps protect an EtherNet/IP connected device from malicious communications.
Security within the system adheres to the
ODVA
CIP Security
standard for usage of cryptographic keys and certificates.

Security

CIP Security
helps protect an EtherNet/IP connected device from malicious communications by:
  • Applying authentication rules and rejecting messages sent by untrusted people or untrusted devices
  • Verifying that data has not been altered during transmission and reject data that fails the integrity check
  • Helping to prevent accessing the EtherNet/IP data by unauthorized parties for additional confidentiality
CIP
-secure policy models support these core security properties:
Property
Description
Device Identity
X.509v3 digital certificates provide cryptographically secure identities to devices.
Device Authentication
The Transport Layer Security (TLS) and Datagram Transport Layer Security (DTLS) cryptographic protocols provide secure transport of EtherNet/IP traffic.
Data Integrity
Hashes or keyed-hash message authentication code (HMAC) provides data integrity and message authenticity to EtherNet/IP traffic.
Data Confidentiality
Data encryption helps prevent accessing the EtherNet/IP data by unauthorized parties.

Authentication methods

CIP
-secure components may use these authentication methods:
Method
Description
Certificate
Established by the use of an X.509v3 certificate granted by a trusted certificate authority.
You can use these options for I/O Data Security if a certificate is used as the authentication method additional security:
Integrity Only
Checks whether data was altered and whether the data was sent by a trusted entity. Altered and/or untrusted data is rejected.
Integrity & Confidentiality
Checks integrity and encrypts the data so the corresponding decryption key is required to read the data. Rejects altered and/or untrusted data.
TIP:
Rockwell Automation
recommends choosing this option.
Pre-shared key
Established by presentation of a shared secret key that is propagated to trusted devices in the system. A pre-shared key can be created manually or
FactoryTalk Policy Manager
can automatically generate pre-shared keys for distribution to the devices in your system.
Trusted IP
Established by identifying an IP address as trusted by the policy model. A set of IP addresses can be defined as a trusted range on your network. Appropriate for use with devices that are not
CIP Security
capable.
For more details about the
CIP
properties available for different policy model components, see:

Conduits

With
CIP
endpoints, you can create these conduits:
CIP
conduits
Endpoint 1
Endpoint 2
Zone
Zone
Zone
Device
Zone
Range
Device
Device
Device
Range
Conduits must follow these rules:
  • Conduits cannot be duplicated, each combination of endpoints must be unique.
  • One of the endpoints must be
    CIP Security
    or
    OPC UA security policy
    capable.
  • If one endpoint is a zone, the other endpoint cannot be a device within that zone.
  • Devices not assigned to any zone or onboarding devices cannot be used as endpoints.

Compatibility

CIP Security
features work with these
Rockwell Automation
products:
  • FactoryTalk Linx
    version 6.11 or later
  • ControlLogix®
    5580 controllers firmware revision 32.00 or later
  • 1756-EN4TR
    ControlLogix
    Module
  • Kinetix®
    5300 Drives
  • Kinetix
    5700 Drives
  • PowerFlex®
    755T
  • 1783-CSP CIP Security Proxy
  • CompactLogix®
    5380 controllers firmware revision 34.00 or later
  • Compact GuardLogix®
    5380 controllers firmware revision 34.00 or later
  • GuardLogix®
    5580 controllers firmware revision 34.00 or later
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal