Enhanced device authentication

Enhanced device authentication
ensures only trusted parties establish connections based on defined policies.

Operation

Enhanced device authentication
adds the Subject Alternative Name (IP address) and may add DNS information unique for a device to its digital identity certificate. This method helps protect against identity spoofing.
You can customize the
enhanced device authentication
to:
  • Receive notifications about devices that do not support
    enhanced device authentication
    .
  • Prohibit the policy deployment to devices that fail
    enhanced device authentication
    .
    IMPORTANT: It is recommended to prohibit the policy deployment to devices that fail
    enhanced device authentication
    .
To enable, disable, or configure
enhanced device authentication
, see Edit Settings.
TIP:
Enabling
enhanced device authentication
involves the deployment of updates to all devices in the policy model. You can deploy the updates directly after enabling
enhanced device authentication
or do that later.

Supported devices

These devices support
enhanced device authentication
:
  • ControlLogix®
    5580 Controllers version 35.00 or later.
  • ControlLogix®
    5580 Process Controllers version 35.00 or later.
  • GuardLogix®
    5580 Controllers version 35.00 or later.
  • CompactLogix®
    5380 Controllers version 35.00 or later.
  • CompactLogix®
    5380 Process Controllers version 35.00 or later.
  • Compact GuardLogix®
    5380 Controllers version 35.00 or later.
  • 1756-EN4TR
    ControlLogix®
    Module.
  • FactoryTalk® Linx
    version 6.40 or later.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal