Edit Settings
Edit
FactoryTalk Policy Manager
Settings to change the policy model name, configure
certificate and ports settings, and enable or disable features.Prerequisites
- Log on toFactoryTalk Policy Manageras an administrator.
- Learn about the available settings. See Settings.
- To Edit Settings
- From the navigation bar, selectSettingsand then select a category of settings.
- Edit fields.TIP: Changes are saved when you select another field or exitSettings.
Provide Feedback