Conduit properties

Use conduit properties to define the endpoints and security settings to apply to communications over this conduit. Endpoints are either a zone, a device, or a port of a device.
Each conduit must be a unique combination of endpoints.

General

Property
Description
Name
Type a name for the conduit.
Description
Type a description for the conduit.

Connection

Property
Description
Endpoint 1
The first endpoint of the conduit. The list is composed of the zones and devices that are identified in
FactoryTalk Policy Manager
.
Endpoint 2
The second endpoint of the conduit.

CIP Security Communication

Property
Description
Authentication Method
Determines how the conduit verifies the identity of the assigned devices and/or zones.
Trusted IP
Devices and zones are trusted for communications based on their IP address. No additional security checks are performed.
Certificate
Devices and zones are trusted by presenting a certificate that establishes their identity.
With this setting selected, configure the
I/O Data Security
and
Messaging Security
settings.
TIP: If an endpoint is a zone and the conduit uses certificate authentication, devices in that zone that do not support
CIP Security
will not use the certificate for communication. The
CIP Security
capable devices will trust the non-
CIP Security
devices using Trusted IP.
I/O Data Security
Determines the type of security check performed on the input and output data.
Integrity Only
This option checks if the data was altered. If detected, rejects altered data.
Integrity & Confidentiality
Checks integrity and encrypts the data so the corresponding decryption key is required to read the data. Rejects altered and/or untrusted data.
None
With this option, no security checks are performed on input and output data.
This setting is available when you choose
Certificate
as the
Authentication Method
.
Messaging Security
Determines the type of security check performed on messages received by assets in the zone.
Integrity Only
This option checks if the data in the message was altered. If detected, rejects altered data
Integrity & Confidentiality
This option checks if the data in the message was altered and that the message was sent by a trusted entity. Rejects the data if it was altered or if it originated from an untrusted entity.
This setting is available when you choose
Certificate
as the
Authentication Method
.

OPC UA

Zones and conduits follow these non-editable
OPC UA security policy
settings:
  • OPC UA
    clients trust
    OPC UA
    servers based on certificates
  • OPC UA
    servers do not trust
    OPC UA
    servers
  • OPC UA
    clients do not trust
    OPC UA
    clients
For more information about
OPC UA
, see OPC UA security policy.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal