Safety
Use safety functionality in FactoryTalk Design Studio to design, verify, and maintain
safety applications.
For a complete description of functional safety in FactoryTalk Design Studio, refer to
the
Develop Safety Applications in FactoryTalk Design Studio Programming
Manual
(publication FTDS-PM001).
NOTE:
When you work with safety functionality in FactoryTalk
Design Studio:
- Any safety system developed using FactoryTalk Design Studio is owned, specified, designed, developed, tested, and validated by the FactoryTalk Design Studio user.
- FactoryTalk Design Studio provides tools to help develop, test, and validate safety applications.
- FactoryTalk Design Studio safety functionality is certified only when used according to the guidance in theDevelop Safety Applications in FactoryTalk Design Studio Programming Manual.
Provide Feedback