Add a safety controller
Add a safety controller to a project to connect the controller with a safety
application. Add controllers from the
Devices
explorer. - On the explorer bar, select
Devices. - InDevicesexplorer, select
, then select
. - InAdd devices to project, underCategory filter, selectSafety.
- Select a safety controller from the list and then selectContinue.
- UnderPending to configure, enter the controller information and then selectFinishto add the controller to the device list.TIP: Controller names:
- Can contain up to 40 valid characters.
- Can contain only alphanumeric characters and underscores.
- Must begin with a letter or underscore.
- Cannot include consecutive underscores.
- Cannot end with an underscore.
TIP: Additional options to add a controller include:- Device list. At the top of theDevice list, select
. - Executionexplorer
. Select
, then select Add controller. InAdd controllers to project, select a controller from the catalog list. - Assigned and Unassigned folders. Right-click on the folders and selectNew device.
TIP:
When you add a safety controller, FactoryTalk
Design Studio creates a safety application with the same name as the controller. See
Create safety applications for more information on
safety applications.
Provide Feedback