Monitor safety status

On a safety controller, use the
Properties > Safety
tab to monitor safety status when you are online. The Safety tab indicates:
  • Safety partner is missing or unavailable (SIL 3).
    A Partnership fault displays in the Safety tab. The pre-deployment check fails if you try to deploy in this condition.
  • Safety partner hardware is incompatible with the primary controller.
    A Partnership fault displays in the Safety tab. The pre-deployment check fails if you try to deploy in this condition.
  • Safety partner firmware is incompatible with the primary controller.
    A Partnership fault displays in the Safety tab. The pre-deployment check fails if you try to deploy in this condition.
  • Safety task inoperable.
    This status is a major safety fault that appears in the Safety tab. Existing fault indications in the Execution Explorer are also applied.
  • Safety task OK.
    No fault or error is reported.
TIP: If the safety project contains a safety partner, select
Safety Partner Information
to view status for the safety partner.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal