Search
FactoryTalk Design Studio Help Center
Programs
A project file is one of the building block of the control system. A program called
Main Program
exists in the Main Task.
Using the software
Create a program
Create FaultHandler program
Create Power Up Handler program
Allocate FactoryTalk Smart Object or program to a controller and task
Monitor program and task properties
Delete a program
Change program class
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal