Change program class
Use the
Properties
panel to change the program class between
Safety and Standard.- On the explorer, from the
Systemview, the
Executionview, or the
Library, select a program. - On thePropertiespane, select theClasslist, and then selectStandardorSafetyas needed.TIP: If the program is inherited from a Smart Object definition, theClassproperty in the Smart Object instance is read-only. Change the class in the Smart Object definition instead.
- InChange program class, selectChange.
Provide Feedback