Select your region

You can select either the
North America
or
Europe
region during initial entitlement allocation. This selection determines where your cloud data is stored and processed.
  1. From
    FactoryTalk Hub
    , select
    Request Access
    .
  2. From Review Entitlements, select
    Confirm Allocation
    .
  3. Select your region that is closest in proximity to your region and select
    Choose the region
    . See Determine your region to learn more about the regions to select. You will be returned to the
    FactoryTalk Design Studio
    Allocation
    . An Allocation successful confirmation message appears.
  4. Go to the
    FT Hub Home
    and select the
    FactoryTalk Design Studio
    card. A waiting room page appears stating that the organization is being provisioned.
  5. When provisioning is complete and the Welcome page appears, select
    Help
    in the upper-right corner of the screen and then select
    About
    .
    About
    displays the selected data center region.
    About
    displays the selected data center region.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal