Search
FactoryTalk Design Workbench Help
Use the high-speed counter instructions
This section provides specific details and examples for using high-speed counter instructions in logic programs, including the following:
Use the high-speed counter instructions
Configure a high-speed counter (HSC) user interrupt
Configure a Programmable Limit Switch
Example: How to create an HSC program
Example: How to add a Programmable Limit Switch (PLS) function
Example: Programmable Limit Switch enabled
HSC instructions
Update HSC application data
New interrupt dialog for HSC
Configure a high-speed counter (HSC) user interrupt
Add and configure a high-speed counter (HSC) user interrupt
Configure a Programmable Limit Switch
Example: How to create an HSC program
Example: Add a Programmable Limit Switch function
Example: Programmable Limit Switch enabled
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal