Configure a high-speed counter (HSC) user interrupt
A user interrupt causes the controller to suspend the task it is performing, perform a different task, and then return to the suspended task at the point where the task was suspended.
L50E and L70E controllers support up to six HSC user interrupts that can be used to execute selected user logic at a pre-configured event.
Provide Feedback