Serial port configuration page
Configure the serial port settings to establish communication between a
Micro800
controller and a serial device.Use the
Serial Port
configuration page to do the following actions:- Configure communication protocols for L20E, L50E, and L70E controllers.
- Select the communication protocol for the serial port.
- Configure the communication settings for the selected communication protocol.
Serial port configuration settings vary with the driver that you selected. Available drivers are as follows:
By default, these serial port settings are not available for an L20E controller that supports remote LCD. To make the settings available, remove the LCD overwrite for serial settings.
Provide Feedback