Configure Asset

To add a new drive the user should provide the following information:
  • Asset Name: Provide a unique name for an asset.
  • Asset Type: Pump, Fan, Blower, Motor (used for other asset types)
  • Manufacturer (optional)
  • Serial number (optional)
  • Model number (optional)
  • Part number (optional)
Configure Asset Parameters
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal