Pump or Fan Specifications
The Number of Blades field is only displayed for the pump or fan selection in the asset type drop down.
- Number of Blades: Integer number entry only. For example, 2. Minimum value is 2 and maximum value is 40.
Provide Feedback