Mobile connectivity

Securely manage the supported
PowerFlex®
devices through the external .

Overview

To set mobile connectivity for the supported devices, provide and set a Pre-Shared Key (PSK) and PSK ID, and then enter those values into the . Deploy the security policy model to enable the device to connect with the . For more information, see Set PSK for mobile connectivity.
TIP: For security reasons, PSK keys are only visible during the set-up. You cannot view PSK keys after the PSK keys are set for mobile connectivity.
Once you set PSK and PSK IDs for mobile connectivity, you can either reset or delete the PSK and PSK ID values, or rename the PSK ID value. For more information, see:
Devices with PSK configured for mobile connectivity display in the
Mobile Connectivity
columns in the tables view. For more information, see Tables.
TIP: Use the
Mobile Connectivity
column or table filters to find devices configured for mobile connectivity.

Compatibility

Mobile connectivity supports these
PowerFlex®
750-Series via Embedded EtherNet/IP devices with firmware revision 12.00 or later in zones with secure communication and certified authentication:
  • PowerFlex®
    755TL drive
  • PowerFlex®
    755TM common bus inverter
  • PowerFlex®
    755TM regenerative bus supply
  • PowerFlex®
    755TR regenerative drive
  • PowerFlex®
    755TS drive
TIP: In
FactoryTalk Policy Manager
, you cannot cut, copy, or paste devices configured for mobile connectivity. You can move such devices between zones with secure communication and certified authentication.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal