Reset PSK for mobile connectivity

Reset Pre-Shared Key (PSK) and PSK ID for the supported
PowerFlex®
750-Series via Embedded EtherNet/IP devices configured for mobile connectivity.
Prerequisites
  1. Ensure that the device is configured for mobile connectivity. See Set PSK for mobile connectivity.
  2. Deploy the security policy model to the device. See Deploy a policy model.
  1. To reset PSK for mobile connectivity
  2. From the navigation bar, either:
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  3. In
    PROPERTIES
    , under
    Mobile connectivity
    , select
    Reset PSK
    .
  4. In
    Set Pre-Shared Key for mobile connectivity
    :
    1. Either generate or enter a unique Pre-Shared Key.
      TIP: PSK must include from 8 to 64 ASCII printable characters.
    2. Either generate or enter a unique Pre-Shared Key ID.
      TIP: PSK ID must include from 1 to 128 ASCII printable characters excluding commas.
      For example, enter
      PSK-mobile-001
    3. Select
      Set PSK and PSK ID
      .
    4. Select either:
      • Copy configuration
        . Copies the IP address, PSK and PSK ID into clipboard.
      • Display QR code with configuration
        . Displays a QR code to scan with your mobile device. Once scanned, the IP address, PSK and PSK ID displays on the mobile device.
        IMPORTANT: Use a secure QR reader from a trusted vendor while working with PSK and PSK IDs.
  5. Enter the new PSK and PSK ID into the .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal